Fort Worth, Texas – June 28, 2022 – TTI, Inc., a leading specialty distributor of electronic components, is stocking TDK’s MEGACAP CKG Series Capacitor. The CKG Series is available as a single MLCC in sizes 1210,1812 and 2220 or as a stacked MLCC in sizes 1812 and 2220. TDK attaches a metal frame to the terminal electrodes of the MLCC which allows excellent resistance to mechanical stress and thermal shock due to the flexibility. The ability to stack the capacitors assists in the reduction of board space allowing for higher capacitance.

The CKG MLCC MEGACAP is offered in 16V to 1000V with these temperature characteristics: C0G, X5R, X7R, X7S and X7T (check the specification sheet for applicable capacitance per characteristic and voltage offerings). The TDK CKG Series is applicable for smoothing and decoupling applications requiring high capacitance.

View all TDK products.

About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 8,000 people in more than 136 locations throughout the Americas, Europe, Asia and Africa. Globally, the TTI Family of Specialists maintain over 3 million square feet of dedicated warehouse space in 30 distribution centers. For more information about TTI, visit www.tti.com

About TDK Corporation
TDK Corporation is a leading electronics company based in Tokyo, Japan. It was established in 1935 to commercialize ferrite, a key material in electronic and magnetic products. TDK's comprehensive portfolio features passive components such as ceramic, aluminum electrolytic and film capacitors, as well as magnetics, high-frequency, and piezo and protection devices. The product spectrum also includes sensors and sensor systems such as temperature and pressure, magnetic, and MEMS sensors. In addition, TDK provides power supplies and energy devices, magnetic heads and more. These products are marketed under the product brands TDK, EPCOS, InvenSense, Micronas, Tronics and TDK-Lambda. TDK focuses on demanding markets in the areas of information and communication technology and automotive, industrial and consumer electronics. The company has a network of design and manufacturing locations and sales offices in Asia, Europe, and in North and South America. In fiscal 2019, TDK posted total sales of USD 12.5 billion and employed about 105,000 people worldwide.