Fort Worth, Texas – June 8, 2022 – TTI, Inc., a leading specialty distributor of electronic components, is now stocking VCNL3036X01 Proximity Sensors from Vishay. These sensors are targeted to meet the requirements of various medical, process automation and industrial sensing applications.

Vishay’s VCNL3036X01 integrates a proximity sensor (PS), a mux and a driver for up to three external IREDs into one small package. It incorporates photodiodes, amplifiers and analog-to-digital converting circuits into a single chip by the CMOS process. PS programmable interrupt features of individual high and low thresholds offer the best utilization of resources and power saving on the microcontroller. These sensors offer a small form factor of 4.0mm x 2.36mm x 0.75mm (L x W x H) and are AEC-Q101 qualified. Key applications include force feedback functions, proximity/optical switches for computing, automotive and industrial devices.

View all Semiconductors / Vishay products.

About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 8,000 people in more than 136 locations throughout the Americas, Europe, Asia and Africa. Globally, the TTI Family of Specialists maintain over 3 million square feet of dedicated warehouse space in 30 distribution centers. For more information about TTI, visit www.tti.com

About Vishay Semiconductor
Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader.