Fort Worth, Texas – June 6, 2022 – TTI, Inc., a leading specialty distributor of electronic components, is stocking Cornell Dubilier’s CMR03-08 Series High Reliability Mica Capacitors. These dipped silvered CMR Mica Capacitors meet the requirement of MIL-PRF-39001 and are ideal for high-grade ground, airborne and spaceborne devices.
CMR MIL-PRF-39001 Capacitors offer stability, high reliability and excellent electrical performance. The CMR03 through 08 are offered in a voltage range of 50Vdc to 500Vdc and a capacitance range of 1 pf to 91,000pf. The CMR offers two temperature ranges: O = –55°C to +125°C and P = –55°C to +150°C. The P temperature range is available only in the CMR04-CMR08.
To learn more, visit CMR High Reliability Mica Capacitors | TTI, Inc.
About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 8,000 people in more than 136 locations throughout the Americas, Europe, Asia and Africa. Globally, the TTI Family of Specialists maintain over 3 million square feet of dedicated warehouse space in 30 distribution centers. For more information about TTI, visit www.tti.com
About Cornell Dubilier
Since its founding in 1909, CDE has been dedicated to advancing capacitor technology for new applications. The company combines innovative products with engineering expertise to provide reliable component solutions for inverters, wind and solar power, electric vehicles, power supplies, motor drives, HVAC, motors, welding, aerospace, telecom, medical equipment and UPS systems. A global company, Cornell Dubilier has ISO-9001 certified manufacturing and distribution facilities in Liberty, SC; New Bedford, MA; Mexicali, Mexico; and Hong Kong.