Fort Worth, Texas – January 26, 2022 – TTI, Inc., a leading specialty distributor of electronic components, has stock for immediate shipment of multiple values of APXG/PXG Series Miniature Solid Conductive Polymer Aluminum Electrolytic Capacitors from United Chemi-Con (UCC). The surface mount APXG/PXG Series has low ESR and is rated for 15,000 hours at 105°C for size codes E61 (5mm), F61 (6.3mm), F80 (6.3mm), H70 (8mm), H80 (8mm) and J80 (10mm). Size codes E46 (5mm) and F45 (6.3mm) are rated for 3,000 hours at 105°C. Available in heights as low as 4.5mm, they are ideal for DC-DC converters, voltage regulators and decoupling applications. Voltage of the APXF Series ranges from 16V to 25V with capacitance ranging from 10µF to 1,000µF.
View all United Chemi-Con products.
About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 7,300 people in more than 136 locations throughout North America, South America, Europe, Asia and Africa. Globally, the company maintains over 3 million square feet of dedicated warehouse space in 30 distribution centers, housing over 850,000 component part numbers. For more information about TTI, visit www.tti.com
About United Chemi-Con
United Chemi-Con, a wholly owned subsidiary of Nippon Chemi-Con, was established in the United States in 1970. The company is the largest manufacturer and supplier of aluminum electrolytic capacitors in North America, with more than 8,000 unique products available.
United Chemi-Con is headquartered in Rolling Meadows, Ill., with manufacturing and warehouse facilities located in Buena Park, Calif., and Lansing, N.C. This—combined with our sales, service and field engineering support throughout the country—ensures customers are met with a superior level of customer service.