Fort Worth, Texas – January 26, 2022 – TTI, Inc., a leading specialty distributor of electronic components, is now stocking the OPB820 family of Transmissive Optical Sensors from TT Electronics - Optek. This sensor is targeted for the medical and industrial applications, manufacturing automation, safety and security equipment.

The TT Electronics - Optek OPB820 device consists of an infrared emitting diode (LED, 890nm center wavelength) and a NPN silicon phototransistor mounted in a robust black plastic housing on opposite sides of an 0.080” (2.03mm) wide slot. Each device in this series has a 0.040” (1.02mm) wide aperture located in front of the infrared diode. Phototransistor switching occurs when an opaque object passes through the slot. These devices are offered with 0.275” (6.96mm) lead spacing for PC board mounting.

View all Optek / TT Electronics products.

About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 7,300 people in more than 136 locations throughout North America, South America, Europe, Asia and Africa. Globally, the company maintains over 3 million square feet of dedicated warehouse space in 30 distribution centers, housing over 850,000 component part numbers. For more information about TTI, visit www.tti.com

About TT Electronics
TT Electronics is a global provider of engineered electronics for performance critical Applications. With around 4,800 employees operating from 29 key locations around the world, TT designs and manufactures a wide range of electronics for sensing, power management and connectivity primarily for applications in the industrial, medical and aerospace and defense sectors. The TT Electronics technology portfolio is one of the most comprehensive in the industry, supplying passive components (fixed and variable resistors, magnetics) and discrete semiconductors (optoelectronics, diodes, MOSFETs) from brands including BI Technologies, IRC, Optek, Semelab and Welwyn Components.