Fort Worth, Texas – January 24, 2022 – TTI, Inc., a leading specialty distributor of electronic components, is now offering G2RG-X Series Relays from OMRON. The G2RG-X Series achieves 500VDC 10A switching capacity when used with 2 pole series wiring. The 3.0mm contact gap offers high insulation with an insulation distance above 8mm and impulse withstand voltage of 10kV between coil and contacts. These components are UL and TÜV certified. Typical applications included include energy storage applications.
About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 7,300 people in more than 136 locations throughout North America, South America, Europe, Asia and Africa. Globally, the company maintains over 3 million square feet of dedicated warehouse space in 30 distribution centers, housing over 850,000 component part numbers. For more information about TTI, visit www.tti.com