Fort Worth, Texas – January 24, 2022 – TTI, Inc., a leading specialty distributor of electronic components, is now stocking the APT1608ZGC Series of Miniature Green LEDs from Kingbright. These LEDs are targeted to meet the indication and illumination requirements of specialty backlighting, corporate branding, handheld devices and medical equipment applications.
Kingbright’s APTD1608 Series LEDs are the industry’s first 0603 dome lens package in Chip LED SMT. The product’s remarkable compact design (1.6mm x 0.8mm x 0.95mm) with 0.70mm dome lens feature focused beams within a narrow viewing angle of 60°, illuminating high typical intensity output up to 3000mcd @ 20mA. Available in blue, white, green, red, yellow and orange, the product’s wide color offerings extend aesthetic benefits for designers of various sign, appliance, interior and exterior automotive lighting, and backlight and indicator applications. The low-power-consumption, IR reflow, solderable device meets industrial temperature ratings of -40°C to +85°C and is specially designed with an automatic, pick-and-place mounting process to reduce production costs. All packages are RoHS compliant and compatible with automated placement equipment to optimize production time and cost.
About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 7,300 people in more than 136 locations throughout North America, South America, Europe, Asia and Africa. Globally, the company maintains over 3 million square feet of dedicated warehouse space in 30 distribution centers, housing over 850,000 component part numbers. For more information about TTI, visit www.tti.com
About Kingbright
Kingbright Company LLC has manufactured innovative Light Emitting Diodes for over 30 years. Kingbright offers the most comprehensive LED product portfolio in the industry, including SMD LEDs, thru-hole LEDs, SMD/through-hole displays, circuit board indicators and high brightness LEDs. Kingbright also offers fully customized LED solutions to enhance customer designs with many options in LED packaging and colors.