Fort Worth, Texas – January 14, 2022 – TTI, Inc., a leading specialty distributor of electronic components, offers Delta Electronics MMCX 50-Ohm Impedance Connector Series RF solutions.
Delta MMCX Series Connectors are microminiature, 50-ohm impedance connectors with snap-on coupling. They are best suited for use with cables in the range of .070" to .120" diameter, such as RG-178 and RG-316/U.
These connectors provide small size, light weight and economy with the convenience of snap-on mating and the ability to rotate connector pairs after mating for precise alignment. Their non-slotted outer contact provides for low RF leakage. All Delta MMCX Connectors are available with gold-plated bodies or with nickel-plated bodies for economy.
To learn more, visit Delta MMCX Connector Series at TTI.
About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 7,300 people in more than 136 locations throughout North America, South America, Europe, Asia and Africa. Globally, the company maintains over 3 million square feet of dedicated warehouse space in 30 distribution centers, housing over 850,000 component part numbers. For more information about TTI, visit www.tti.com
About Delta Electronics Manufacturing Corp.
Delta Electronics Mfg. Corp. is a third-generation, family owned business, that has been advancing Connector Technology Since 1955. With Full vertical manufacturing capabilities including CNC machining, electroplating, assembly, and test and measurement, they have accumulated over 75 years of engineering experience. Delta Electronics has vector network analyzer capabilities up to 65 GHz and specializes in rapid response to custom design and application assistance. Delta Electronics is proud to have state-of-the-art design and analysis tools, including Ansoft HFSS, even more so, Delta Electronics is proud to be environmentally conscious and RoHS compliant.