Fort Worth, Texas – January 11, 2022 – TTI, Inc., a leading specialty distributor of electronic components, is now offering the G5PZ Power PCB Relay from OMRON.

This slim, space-saving relay is smaller in comparison to relays of the same class. It is available in 16A 250VAC and a high-capacity version rated at 20A 250VAC. The high-sensitivity 530mW coil offers further energy savings with a 50 percent holding voltage. Typical applications include home appliances, office automation equipment as well as industrial machinery.

To learn more, visit Aratas PCB Relay at TTI.

About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 7,300 people in more than 136 locations throughout North America, South America, Europe, Asia and Africa. Globally, the company maintains over 3 million square feet of dedicated warehouse space in 30 distribution centers, housing over 850,000 component part numbers. For more information about TTI, visit www.tti.com