Fort Worth, Texas – January 7, 2022 – TTI, Inc., a leading specialty distributor of electronic components, has stock for immediate shipment of multiple values of the SMCJ Series Surface Mount Transient Voltage Suppressors from Vishay. These devices are rated for 1500W peak pulse power dissipation (10/1000 μs waveform) and are available in standoff voltages from 5.0V to 188V. The SMCJ Series is available in the SMC (DO-214AB) package in both unidirectional and bi-directional versions. Typical applications include use in sensitive electronics for protection against voltage transients. An AEC-Q101-qualified version is available.
For more information, visit Vishay SMCJ Series 1500W TVS Diodes at TTI.
About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 7,300 people in more than 136 locations throughout North America, South America, Europe, Asia and Africa. Globally, the company maintains over 3 million square feet of dedicated warehouse space in 30 distribution centers, housing over 850,000 component part numbers. For more information about TTI, visit www.tti.com
About Vishay Intertechnology
Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, rectifiers, MOSFETs, optoelectronics, and selected ICs) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.