Fort Worth, Texas – January 5, 2022 – TTI, Inc., a leading specialty distributor of electronic components, is now stocking Dialight’s 515-1301-03 Series Flat Faced Light Pipes. These ruggedized light pipes are designed to utilize a PCB-mounted LED for optimum light transmission.
Dialight’s 515-1301-03 Flat Light Pipes are a standard design intended for overall length of 0.300 inches, with a recommended minimum of 0.200 inches between light pipes as a normal mounting pitch. This light pipe is held in place by two press-fit pins along the bottom of the device. The light pipe is not attached to the panel at any point but can protrude through holes in the panel. The 0.093-inch diameter light pipe material is water-clear transmissive polycarbonate rated UL94-V0 and has a 35 percent oxygen index.
To learn more, visit Dialight Flat Mount Light Pipes at TTI.
About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 7,300 people in more than 136 locations throughout North America, South America, Europe, Asia and Africa. Globally, the company maintains over 3 million square feet of dedicated warehouse space in 30 distribution centers, housing over 850,000 component part numbers. For more information about TTI, visit www.tti.com
About Dialight
Dialight is the world leader in LED technology with millions of LED fixtures and indicators installed worldwide. The company began in 1938 in Brooklyn, NY, where they produced instrument panel lights for aircraft. In 1971 Dialight launched the first LED Circuit Board Indicators. Dialight has revolutionized the use of LEDs to provide superior lighting for traffic control, indicators, structural towers and industrial sites around the world.