Fort Worth, Texas – January 5, 2022 – TTI, Inc., a leading distributor of electronic components, has stock for immediate shipment of multiple values of the SMCJ Series of TVS Suppressor Diodes from Bourns. The SMCJ Series is offered in the compact DO-214AB (SMC) size format and is rated for 1500 watts minimum peak pulse power dissipation. Working peak reverse voltage is available from 5V up to 495V, and typical fast response times are less than 1.0 picosecond for unidirectional devices and less than 5.0 picoseconds for bidirectional devices from 0V to minimum breakdown voltage. Peak forward surge current is 200A with 5 watts steady state power dissipation.
For more information, visit Bourns SMCJ 1500W TVS Diodes at TTI.
About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 7,300 people in more than 136 locations throughout North America, South America, Europe, Asia and Africa. Globally, the company maintains over 3 million square feet of dedicated warehouse space in 30 distribution centers, housing over 850,000 component part numbers. For more information about TTI, visit www.tti.com
About Bourns
Bourns, Inc., is a leading manufacturer and supplier of position and speed sensors, circuit protection solutions, magnetic components, microelectronic modules, panel controls and resistive products. Headquartered in Riverside, California, USA, Bourns serves a broad range of markets, including automotive, industrial, consumer, communications, non-critical life support medical, audio and various other market segments. Additional company and product information is available at www.bourns.com.