Fort Worth, Texas – January 4, 2022 – TTI, Inc., a leading specialty distributor of electronic components, announces the availability of the full range of Micro-One Wire-to-Board Connector with TPA (terminal position assistance) from stock at TTI.
Molex now adds a TPA option to its Micro-One Wire-to-Board Connectors. The range also features ISL for improved mating and contact retention in high-vibration applications. The low-profile, 2.00mm pitch design is compatible with the existing and proven MicroClasp terminals and tooling. Micro-One Series Connectors are ideal for use in a variety of consumer and industrial applications, to name but a few.
About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 7,300 people in more than 136 locations throughout North America, South America, Europe, Asia and Africa. Globally, the company maintains over 3 million square feet of dedicated warehouse space in 30 distribution centers, housing over 850,000 component part numbers. For more information about TTI, visit www.tti.com