Fort Worth, Texas – January 3, 2022 – TTI, Inc., a leading specialty distributor of electronic components, has stock for immediate shipment of multiple values of the United Chemi-Con ELXS/LXS Series Snap-In Aluminum Electrolytic Capacitors. Capacitance of the ELXS/LXS Snap-In Series ranges from 82µF up to 3,300µF. The ELXS/LXS Series is rated for 5,000 hours at 105°C and is available in voltages from 160VDC up to 600VDC. Case diameters range from 22mm up to 35mm and lengths range from 25mm up to 60mm.
To learn more, visit UCC ELXS/LXS Series Long Life Aluminum Snap-in Caps at TTI.
About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 7,300 people in more than 136 locations throughout North America, South America, Europe, Asia and Africa. Globally, the company maintains over 3 million square feet of dedicated warehouse space in 30 distribution centers, housing over 850,000 component part numbers. For more information about TTI, visit www.tti.com
About United Chemi-Con
United Chemi-Con, a wholly owned subsidiary of Nippon Chemi-Con, was established in the United States in 1970. The company is the largest manufacturer and supplier of aluminum electrolytic capacitors in North America, with more than 8,000 unique products available. United Chemi-Con is headquartered in Rolling Meadows, Ill., with manufacturing and warehouse facilities located in Buena Park, Calif., and Lansing, N.C. This—combined with our sales, service and field engineering support throughout the country—ensures customers are met with a superior level of customer service.