Fort Worth, Texas – January 3, 2022 – TTI, Inc., a leading specialty distributor of electronic components, is now stocking the Rohm BD8379FV-M LED driver series. These LED drivers are optimized for use in indication and illumination systems for display clusters, digital signage, industrial backlighting, and medical systems.

Rohm’s BD8379FV-M is a serial-in parallel-out controlled LED driver with 35V output voltage rating. With the input of 3-line serial data, it turns the 12ch open drain output on/off. Due to its compact size, it is optimal for compact space designs. Featuring open drain output, 3-line serial control + enable signal, and cascade connection compatible. Rohm’s new product is compatible with standard reflow soldering processes, environmentally friendly, RoHS-compliant, halogen-free and AEC-Q100 Qualified.

To learn more, visit Rohm 12 Channel LED Driver at TTI.

About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 7,300 people in more than 136 locations throughout North America, South America, Europe, Asia and Africa. Globally, the company maintains over 3 million square feet of dedicated warehouse space in 30 distribution centers, housing over 850,000 component part numbers. For more information about TTI, visit www.tti.com


About Rohm Semiconductor
ROHM offers a full line of leading-edge sensors, silicon carbide MOSFETs and Schottky barrier diodes, optoelectronics, and power management ICs. If you’re designing for rugged environments requiring high-temperature and/or high-voltage along with higher power density solutions – TTI is fully franchised for ROHM, Kionix MEMS Sensors and accelerometers, and LAPIS Semiconductor products.