Fort Worth, Texas – February 24, 2022 – TTI, Inc., a leading specialty distributor of electronic components, is now offering the SIM-20ST family of Infrared LEDs from ROHM Semiconductor. These emitters are targeted for specialty infrared illumination and sensing applications such as medical instruments, industrial and manufacturing automation, safety and security equipment.

ROHM’s SIM-20ST family of infrared emitters are uniquely suited for specialty sensing of target presence or motion in limited spacing applications. They include highly efficient 950nm LED die for maximum IR power in low voltage and battery powered products and are built in a 15-degree emission half-angle. Operating temperatures range from -40°C to +85°C for industrial product operation.

To learn more, visit ROHM Semiconductor SIM-20ST Emitters at TTI.

About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 8,000 people in more than 136 locations throughout the Americas, Europe, Asia and Africa. Globally, the TTI Family of Specialists maintain over 3 million square feet of dedicated warehouse space in 30 distribution centers. For more information about TTI, visit www.tti.com

About ROHM Semiconductor
ROHM offers a full line of leading-edge sensors, silicon carbide MOSFETs and Schottky barrier diodes, optoelectronics, and power management ICs. If you’re designing for rugged environments requiring high-temperature and/or high-voltage along with higher power density solutions. ROHM’s product family includes ROHM Semiconductor, Kionix MEMS Sensors and accelerometers, and LAPIS Semiconductor products.