Fort Worth, Texas – February 21, 2022 – TTI, Inc., a leading specialty distributor of electronic components, is now stocking the G8PM Relay from OMRON. The High Power G8PM Relay is suited for 12VDC motor and resistive control applications and can support a 60A fuse. Its small size and heat resistance enable usage in the engine compartment. It has a temperature range of -40°C to +125°C and is pin-in-paste compliant. Typical applications include motor and resistive application control, headlights, main power, EPS and DC/DC converters.
View all OMRON products.
About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 8,000 people in more than 136 locations throughout the Americas, Europe, Asia and Africa. Globally, the TTI Family of Specialists maintain over 3 million square feet of dedicated warehouse space in 30 distribution centers. For more information about TTI, visit www.tti.com