Fort Worth, Texas – February 14, 2022 - TTI, Inc., a leading specialty distributor of electronic components, has stock for immediate shipment of Vishay’s TrenchFET® Si1308EDL 30V N-Channel MOSFET in the compact SOT-323/SC-70 surface mount package. The three-leaded SC-70 package measures 2.0mm x 2.1mm and has a continuous drain current of 1.4A. Applications include DC/DC converters, boost converters and load switches. Maximum power dissipation of the Si1308EDL is 0.5W. Drain-source on-state resistance is a very low 0.110 ohms and total gate charge is 2.7nC.
For more information, visit Vishay Si1308EDL 30V N-Channel MOSFET at TTI.
About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 8,000 people in more than 136 locations throughout the Americas, Europe, Asia and Africa. Globally, the TTI Family of Specialists maintain over 3 million square feet of dedicated warehouse space in 30 distribution centers. For more information about TTI, visit www.tti.com
About Vishay Intertechnology
Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, rectifiers, MOSFETs, optoelectronics, and selected ICs) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.