Fort Worth, Texas – February 11, 2022 – TTI, Inc., a leading specialty distributor of electronic components, has stock for immediate shipment of the small footprint 2N7002NXBK MOSFET from Nexperia. The N-Channel 2N7002NXBK is in the popular SOT23 package and measures only 2.9mm x 2.3mm x 1.0mm. Drain-source voltage is 60V and drain current is 270mA. The 2N7002NXBK is fast switching and logic-level compatible. Applications include relay drivers, high speed line drivers, low-side load switches and switching circuits.
About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 8,000 people in more than 136 locations throughout the Americas, Europe, Asia and Africa. Globally, the TTI Family of Specialists maintain over 3 million square feet of dedicated warehouse space in 30 distribution centers. For more information about TTI, visit www.tti.com
About Nexperia
Nexperia is a leading expert in the high-volume production of essential semiconductors, components that are required by every electronic design in the world. The company’s extensive portfolio includes diodes, bipolar transistors, ESD protection devices, MOSFETs, GaN FETs and analog & logic ICs. We became independent at the beginning of 2017. Focused on efficiency, Nexperia produces consistently reliable semiconductor components at high volume: more than 90 billion annually. Our extensive portfolio meets the stringent standards set by the automotive industry. And industry-leading small packages, produced in our own manufacturing facilities, combine power and thermal efficiency with best-in-class quality levels. Built on over half a century of expertise, Nexperia has over 12,000 employees across Asia, Europe and the U.S. supporting customers globally.