Fort Worth, Texas – August 10, 2022 – TTI, Inc., a leading specialty distributor of electronic components, is now stocking Dialight’s 552 Dual Color Indicators. These LED Indicators are designed to meet the lighting needs of industrial, storage compartments and network equipment applications.
The 552 Series Dual Color Indicators are designed with a highly durable housing and are designated for a variety of applications such as instrument panels, gauges, dash boards, storage compartments and control panels. Ideal for a variety of applications such as main power indication, remote power indication and status indication, these indicators operate at 2–5 VDC with no resistor required and feature a wide operating temperature range of -55°C to +100°C for excellent harsh environment performance.
About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 8,000 people in more than 136 locations throughout the Americas, Europe, Asia and Africa. Globally, the TTI Family of Specialists maintain over 3 million square feet of dedicated warehouse space in 30 distribution centers. For more information about TTI, visit www.tti.com
About Dialight
Dialight is the world leader in LED technology with millions of LED fixtures and indicators installed worldwide. The company began in 1938 in Brooklyn, NY, where they produced instrument panel lights for aircraft. In 1971 Dialight launched the first LED Circuit Board Indicators. Dialight has revolutionized the use of LEDs to provide superior lighting for traffic control, indicators, structural towers and industrial sites around the world.