Fort Worth, Texas – August 10, 2022 – TTI, Inc., a leading specialty distributor of electronic components, is now stocking Dialight’s 515-1302 Series of Optopipe® Panel Mount Light Pipes. These ruggedized light pipes are designed as front panel indicators and utilize a PCB-mounted LED for optimum light transmission.
Dialight’s 515-1302 Convex Lensed Light Pipes are offered as a standard design with various length options of 0.125 inches to 1.25 inches. With a recommended minimum of 0.200 inches between light pipes as a normal mounting pitch, these light pipes are held in place by two press-fit pins along the bottom of the body. The light pipe is not attached to the panel at any point but can protrude through holes in the panel. The 0.115-inch diameter light pipe material is water clear transmissive polycarbonate rated UL94-V0, RoHS and has a 35 percent oxygen index. They are specifically designed for front panel indication in industrial, medical and networking equipment.
About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs has established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Specialists, Mouser Electronics, Sager Electronics and the Exponential Technology Group employ over 8,000 people in more than 136 locations throughout the Americas, Europe, Asia and Africa. Globally, the TTI Family of Specialists maintain over 3 million square feet of dedicated warehouse space in 30 distribution centers. For more information about TTI, visit www.tti.com
About Dialight
Dialight is the world leader in LED technology with millions of LED fixtures and indicators installed worldwide. The company began in 1938 in Brooklyn, NY, where they produced instrument panel lights for aircraft. In 1971 Dialight launched the first LED Circuit Board Indicators. Dialight has revolutionized the use of LEDs to provide superior lighting for traffic control, indicators, structural towers and industrial sites around the world.