Fort Worth, Texas – May 15, 2020 – TTI, Inc., a leading specialty distributor of electronic components, is stocking the FP1308 Series Inductors from EATON. 

Eaton FP1308R high current, high frequency power inductors feature controlled DC Resistance for sensing circuits, a frequency range up to 2MHz, an inductance range from 110nH to 440nH, and a current range from 37 to 120 Amps. The FP1308R series comes in a 12.70 x 13.46 x 8.0mm Flat-Pac™ surface mount package with ferrite core material. These devices are halogen free, RoHS compliant and have a maximum operating temperature of 125°C.

The EATON FP1308R series power inductors are ideal for industrial IoT applications, battery power systems, point-of-load modules, DCR sensing, and much more.

About TTI

TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of interconnect, passive and electromechanical (IP&E) components and the distributor of choice for industrial and consumer electronics manufacturers worldwide. Broader and deeper inventory, leading-edge products and custom supply chain solutions have established TTI as the leading specialist in electronic component distribution. Globally, the company maintains over 2 million square feet of dedicated warehouse space containing over 850,000 component part numbers. Along with its subsidiaries, Mouser Electronics, Sager Electronics, and TTI Semiconductor Group, TTI employs more than 7,000 people at more than 133 locations throughout North America, South America, Europe, Asia and Africa. For more information about TTI, visit www.ttiinc.com

About EATON

At Eaton, we're dedicated to improving people's lives and the environment with power management technologies that are more reliable, efficient, safe and sustainable. We are a power management company made up of over 97,000 employees, doing business in more than 175 countries.