Fort Worth, Texas – June 30, 2020 – TTI, Inc., a leading specialty distributor of electronic components, is offering the 100B and 1000B Series Ethernet Transformers from PulseR Ruggedized Solutions.
PulseR’s 100B/1000B Ethernet ruggedized transformers are made with transfer molded or pour filled construction to meet MIL-PRF-21038 environment requirements. They support AFDX (Avionics Full Duplex Switched Ethernet), TTE (Time Triggered Ethernet) and IEEE 802.3x including PoE (Power over Ethernet). This family has extended operating temperature options of -55°C to +125°C, maximum isolation voltage of 2500 VDC and 1800VAC and are AS9100C Certified.
The PulseR 100B/1000B Ethernet Transformers are military and aerospace grade devices that are designed for ruggedized applications such as satellites, aircraft and land-based mobile communications units.
View all Pulse Electronics products.
About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of interconnect, passive and electromechanical (IP&E) components and the distributor of choice for industrial and consumer electronics manufacturers worldwide. Broader and deeper inventory, leading-edge products and custom supply chain solutions have established TTI as the leading specialist in electronic component distribution. Globally, the company maintains over 2 million square feet of dedicated warehouse space containing over 850,000 component part numbers. Along with its subsidiaries, Mouser Electronics, Sager Electronics, and TTI Semiconductor Group, TTI employs more than 7,000 people at more than 133 locations throughout North America, South America, Europe, Asia and Africa. For more information about TTI, visit www.ttiinc.com
About PulseR
PulseR, LLC is a world-class manufacturer of catalog and custom magnetic components with both domestic and offshore manufacturing facilities. Our products serve the Military, Commercial Aerospace, Manned and Unmanned Space, High-reliability Industrial, Medical, Transportation, and Power-Grid Infrastructure markets across the globe.
For over 70 years, PulseR’s experienced engineering teams have offered cutting-edge technical solutions while our manufacturing expertise provides comprehensive production. PulseR’s award-winning quality and service will exceed demanding customer expectations – no matter the mission.