Fort Worth, Texas – June 29, 2020 – TTI, Inc., a leading specialty distributor of electronic components, is offering Ceramic Resonators from Abracon.
Abracon’s Ceramic Resonators are available in a wide resonant frequency range with low resonant impedance as low as 30Ω at 16MHz. These resonators are available with built-in capacitance options of 5, 10, 15, 22, 30, 33, 39 or 47 pF in a variety of industry standard footprints and also available in a wide operating temperature range of up to -40 to +125°C.
Abracon Ceramic Resonators are designed for ruggedized applications such as remote metering systems, industrial IoT appliances and communication equipment.
About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of interconnect, passive and electromechanical (IP&E) components and the distributor of choice for industrial and consumer electronics manufacturers worldwide. Broader and deeper inventory, leading-edge products and custom supply chain solutions have established TTI as the leading specialist in electronic component distribution. Globally, the company maintains over 2 million square feet of dedicated warehouse space containing over 850,000 component part numbers. Along with its subsidiaries, Mouser Electronics, Sager Electronics, and TTI Semiconductor Group, TTI employs more than 7,000 people at more than 133 locations throughout North America, South America, Europe, Asia and Africa. For more information about TTI, visit www.ttiinc.com
About Abracon
Abracon is a leading global manufacturer of passive and electromechanical timing, synchronization, power, connectivity and RF solutions. Focused on customer service, support, innovation, quality and on-time delivery, Abracon supports over 25,000 active customers and ships over a quarter billion components each year.