Fort Worth, Texas – June 24, 2020 – The UCC MZL Series Aluminum Electrolytic Caps are now available from TTI, Inc., a leading specialty distributor of electronic components. The MZL series is rated for 5,000 hours at 105°C. It is available in a surface mount package with an option for a vibration-resistant version. Voltage of the MZL series ranges from 6.3V to 50V with capacitance ranging from 100µF to 1,500µF. An AECQ-200 version is also available.
To learn more, visit UCC MZL Series at TTI.
About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of interconnect, passive and electromechanical (IP&E) components and the distributor of choice for industrial and consumer electronics manufacturers worldwide. Broader and deeper inventory, leading-edge products and custom supply chain solutions have established TTI as the leading specialist in electronic component distribution. Globally, the company maintains over 2 million square feet of dedicated warehouse space containing over 850,000 component part numbers. Along with its subsidiaries, Mouser Electronics, Sager Electronics, and TTI Semiconductor Group, TTI employs more than 7,000 people at more than 133 locations throughout North America, South America, Europe, Asia and Africa. For more information about TTI, visit www.ttiinc.com
About United Chemi-Con
United Chemi-Con, a wholly owned subsidiary of Nippon Chemi-Con, was established in the United States in 1970. The company is the largest manufacturer and supplier of aluminum electrolytic capacitors in North America, with more than 8,000 unique products available.
United Chemi-Con is headquartered in Rolling Meadows, Ill., with manufacturing and warehouse facilities located in Buena Park, Calif., and Lansing, N.C. This—combined with our sales, service and field engineering support throughout the country—ensures customers are met with a superior level of customer service.