Fort Worth, Texas – April 21, 2020 – TTI, Inc., a leading distributor of electronic components is stocking Eaton’s PolySurg™ ESD suppressors. With a typical capacitance of 0.05pF, PolySurg devices are ideal for high speed data applications like USB 2.0/3.0, IEEE 1394, DVI, and high-speed Ethernet. The fast response time of the devices (<1ns) allows equipment to pass IEC 61000-4-2 level 4 testing. The suppressors are available in single line devices as small as 0402 (1005 metric) and 0603 (1608 metric) as well as four-line arrays (41206ESDA).
The PS04LTVA1 device is tested to meet automotive specifications (AEC-Q200). Additionally, the low trigger voltage and clamping voltage delivers enhanced ESD protection of very sensitive ICs and the low leakage current (<0.1nA typ.) reduces power consumption. To learn more visit Eaton PolySurg or Eaton PS04LTVA1 at TTI.
About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of interconnect, passive and electromechanical (IP&E) components and the distributor of choice for industrial and consumer electronics manufacturers worldwide. Broader and deeper inventory, leading-edge products and custom supply chain solutions have established TTI as the leading specialist in electronic component distribution. Globally, the company maintains over 2 million square feet of dedicated warehouse space containing over 850,000 component part numbers. Along with its subsidiaries, Mouser Electronics, Sager Electronics, and TTI Semiconductor Group, TTI employs more than 7,000 people at more than 133 locations throughout North America, South America, Europe, Asia and Africa. For more information about TTI, visit www.ttiinc.com
About Eaton
Eaton is a power management company with 2018 sales of $21.6 billion. We provide energy-efficient solutions that help our customers effectively manage electrical, hydraulic and mechanical power more efficiently, safely and sustainably. Eaton is dedicated to improving the quality of life and the environment through the use of power management technologies and services. Eaton has approximately 99,000 employees and sells products to customers in more than 175 countries.