Fort Worth, Texas – April 17, 2020 – TTI, Inc., a leading specialty distributor of electronic components, is now stocking the VCNL36 family of proximity sensors from Vishay. These sensors are targeted to meet the requirements of various medical, IOT and industrial applications. 

These fully integrated proximity sensors include a high power VCSEL coupled with a photodiode for presence and proximity sensing in an SMD package. They incorporate the photodiodes, amplifiers, and analog to digital conversion circuits into a single CMOS ASIC. Having sensing ranges of up to 20cm (7.9 in) at 20 mA pulsed current where other sensors need up to 200 mA. With no need for mechanically isolating the emitter and detector these components significantly simplify the design-in process. The LLC surface mount packages with a low profile 1mm height makes them a perfect candidate for tight spaces with minimal real-estate requirements. 

These sensors include a program interrupt function through their I2C bus serial interface. This allows for easy access to the “proximity signal” to utilize the wake-up function in the microprocessor when a proximity change occurs, which is helpful in reducing the overall processing overhead and power requirements. Average current consumption at MAX forward current is 0.80 mA making them well suited for battery operated and power sensitive applications.

VCNL36 products have an unlimited shelf life. Compatible with reflow solder processes according to JEDEC-STD-020D, the devices are RoHS-compliant, halogen-free, and Vishay Green.

To learn more, search parts for Vishay Proximity Sensors.

About TTI

TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of interconnect, passive and electromechanical (IP&E) components and the distributor of choice for industrial and consumer electronics manufacturers worldwide. Broader and deeper inventory, leading-edge products and custom supply chain solutions have established TTI as the leading specialist in electronic component distribution. Globally, the company maintains over 2 million square feet of dedicated warehouse space containing over 850,000 component part numbers. Along with its subsidiaries, Mouser Electronics, Sager Electronics, and TTI Semiconductor Group, TTI employs more than 7,000 people at more than 133 locations throughout North America, South America, Europe, Asia and Africa. For more information about TTI, visit www.ttiinc.com

About Vishay Semiconductor

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets.