Fort Worth, Texas – April 15, 2020 – TTI, Inc., a leading specialty distributor of electronic components, has available inventory for AVX hybrid and electric vehicle film capacitors. AVX produces a full range of film dielectric components – from low power SMD solutions for the commercial and automotive industry, to medium and high-power film capacitors suited to all power electronic applications over a voltage range spanning 75V volts up to 100 kV. All AVX capacitors are available through TTI. The FHC1 & FHC2 series capacitors are AEC-Q qualified and have been specially designed to be used in conjunction with Hybrid & Electric vehicles IGBT modules.

The AVX FHC series provides a standard option for DC link capacitors used in DC filtering between rectifier and inverter in automotive applications. The series uses a dry-wound (non-oil-filled) segmented metallized polypropylene, specially treated to have a very high dielectric strength in operating conditions up to 115°C. Voltages range from 300VDC up to 1,400VDC with capacitance values ranging from 100μF – 1,500μF.

Search KYOCERA AVX Film Capacitors

About TTI

TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of interconnect, passive and electromechanical (IP&E) components and the distributor of choice for industrial and consumer electronics manufacturers worldwide. Broader and deeper inventory, leading-edge products and custom supply chain solutions have established TTI as the leading specialist in electronic component distribution. Globally, the company maintains over 2 million square feet of dedicated warehouse space containing over 850,000 component part numbers. Along with its subsidiaries, Mouser Electronics, Sager Electronics, and TTI Semiconductor Group, TTI employs more than 7,000 people at more than 133 locations throughout North America, South America, Europe, Asia and Africa. For more information about TTI, visit www.ttiinc.com