Fort Worth, Texas – April 13, 2020 – TTI, Inc., a leading specialty distributor of electronic components, is now stocking a wide variety of infrared emitters and detectors from Kingbright. These LEDs are targeted for unique sensing applications in medical and Industrial equipment. 

Kingbright introduces the expanded IR LEDs and Phototransistors in industry standard SMD and through-hole packages. Kingbright IR LEDs selection features infrared emitters and phototransistors in wavelength ranges from 880nm to 940nm @ 20mA (or *50mA) with different lens options and viewing angles from 20° to 160°. This selection offers multiple package alternatives which include PLCC, subminiature, top emitting, right angle, dome lens SMD LEDs, as well as 3mm and 5mm through-hole in matching emitter/detector pairs.

To further broaden our product offering, Kingbright introduces ambient light photo sensors and RGB color sensors. The ambient light photo sensor is a NPN silicon phototransistor which is adapted to respond similar to the human eye. Sensitive to visible spectrums, it is an effective power saving solution to display backlighting appliances. The RGB color sensor uses three Si photodiodes with color filter, which makes it an ideal solution to color balance of display backlighting appliances. Both sensors are available in standard SMD packages.

View all Kingbright products.

About TTI

TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of interconnect, passive and electromechanical (IP&E) components and the distributor of choice for industrial and consumer electronics manufacturers worldwide. Broader and deeper inventory, leading-edge products and custom supply chain solutions have established TTI as the leading specialist in electronic component distribution. Globally, the company maintains over 2 million square feet of dedicated warehouse space containing over 850,000 component part numbers. Along with its subsidiaries, Mouser Electronics, Sager Electronics, and TTI Semiconductor Group, TTI employs more than 7,000 people at more than 133 locations throughout North America, South America, Europe, Asia and Africa. For more information about TTI, visit www.ttiinc.com