Fort Worth, Texas – April 9, 2020 – TTI, Inc., a leading specialty distributor of electronic components, is now stocking an expanded offering of Rohm Infrared LEDs. These products are available in both through hole and surface mount packages. Currently available in 850nm – 870nm wave lengths to fit your design requirements.

These infrared LEDs are suitable for many non-contact sensing applications especially for medical and industrial products. With automotive quality built in, they are well suited for medical equipment sensing needs like ECG/(EKG) equipment, pulse oximeters, digital stethoscopes, blood glucose meters, blood pressure monitoring and ultrasound systems.

Rohm also offers a variety of spectrally matched sensors in phototransistor and photodiode output configurations. They are offered in both through hole and surface mount options as well. This makes it possible to design in matched optical characteristics, significantly easing the design challenges.

Additionally, by optimizing the LED die, ROHM was able to improve intensity and overall reliability. Most of these LEDs are AEC-Q101 qualified, making them suitable for the ever-increasing medical equipment requirements.

View all ROHM Semiconductor products.

About TTI

TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of interconnect, passive and electromechanical (IP&E) components and the distributor of choice for industrial and consumer electronics manufacturers worldwide. Broader and deeper inventory, leading-edge products and custom supply chain solutions have established TTI as the leading specialist in electronic component distribution. Globally, the company maintains over 2 million square feet of dedicated warehouse space containing over 850,000 component part numbers. Along with its subsidiaries, Mouser Electronics, Sager Electronics, and TTI Semiconductor Group, TTI employs more than 7,000 people at more than 133 locations throughout North America, South America, Europe, Asia and Africa. For more information about TTI, visit www.ttiinc.com

About Rohm Semiconductor

ROHM offers a full line of leading-edge sensors, silicon carbide MOSFETs and Schottky barrier diodes, infrared optoelectronics, and power management ICs. If you’re designing for rugged environments requiring high-temperature and/or high-voltage along with higher power density solutions.