Fort Worth, Texas – April 9, 2020 – TTI, Inc., a leading specialty distributor of electronic components, is now offering the Murata DLW32MH201 family of common mode chokes from Murata.
The Murata DLW32MH201 Family of Inductors, available from TTI Inc., is a common mode choke coil (CMCC) for Automotive Ethernet. These inductors have an 80V rating, are in a 1210 package, (3.2 mm x 2.5 mm), have an operating range from -55 to +150°C, and are compliant to AEC-Q200 standard. This product is a world first for its type and is perfect for harsh temperature environments.
In recent years, as cars have been equipped with more advanced features, the number of Engine Control Units (ECU) installed in cars has been increasing in order to support the functioning of autonomous driving systems such as ADAS. As networks for connecting these ECUs, high-speed interfaces that support the differential signal transmission systems like Automotive Ethernet are becoming common. Along with this trend, there is a growing need for components that can be used in high-temperature environments such as engine rooms.
Search Murata DLW32MH201 Automotive Common-Mode Chokes
About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of interconnect, passive and electromechanical (IP&E) components and the distributor of choice for industrial and consumer electronics manufacturers worldwide. Broader and deeper inventory, leading-edge products and custom supply chain solutions have established TTI as the leading specialist in electronic component distribution. Globally, the company maintains over 2 million square feet of dedicated warehouse space containing over 850,000 component part numbers. Along with its subsidiaries, Mouser Electronics, Sager Electronics, and TTI Semiconductor Group, TTI employs more than 7,000 people at more than 133 locations throughout North America, South America, Europe, Asia and Africa. For more information about TTI, visit www.ttiinc.com
About Murata
Murata is a global leader in the design, manufacture and supply of advanced electronic materials, leading edge electronic components, and multi-functional, high-density modules. Murata innovations can be found in a wide range of applications from mobile phones to home appliances, and automotive applications to energy management systems and healthcare devices.