Fort Worth, Texas, April 2, 2020 –TTI, Inc., a leading specialty distributor of electronic components, is now offering the IHDM Automotive Grade Inductors from Vishay. 

The Vishay IHDM inductor family, available from TTI, Inc., enables current ratings up to 150 Amps with a powdered iron alloy core technology. This trough-hole inductor family provides stable inductance and saturation over a demanding operating temperature from -40 °C to +180 °C with low power losses and excellent heat dissipation.

This family is designed for under the hood applications in hybrid, full-electric and hydrogen fuel cell vehicles. With an operating voltage up to 350V, they are ideal for high current, high temperature power applications, including DC/DC converter, inverters, and filter for motor and switching noise suppression.

Search Vishay IHDM Inductors

About TTI

TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of interconnect, passive and electromechanical (IP&E) components and the distributor of choice for industrial and consumer electronics manufacturers worldwide. Broader and deeper inventory, leading-edge products and custom supply chain solutions have established TTI as the leading specialist in electronic component distribution. Globally, the company maintains over 2 million square feet of dedicated warehouse space containing over 850,000 component part numbers. Along with its subsidiaries, Mouser Electronics, Sager Electronics, and TTI Semiconductor Group, TTI employs more than 7,000 people at more than 133 locations throughout North America, South America, Europe, Asia and Africa. For more information about TTI, visit www.ttiinc.com

About Vishay (manufacturer)

Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, rectifiers, MOSFETs, optoelectronics, and selected ICs) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.