Fort Worth, Texas – April 2, 2020 – TTI, Inc., a leading specialty distributor of electronic components, is offering the CLTM12-S series from Carling Technologies. The CLTM12-S is a solid-state load controller with 12 high-side outputs, four digital inputs, three discrete inputs, two address lines, and a CAN baud rate select line. It provides fast, low-loss, solid-state on/off switching along with short circuit protection for each output, as well as load status and power diagnostics.

Relative to electromechanical relays, the CLTM12-S increases thermal efficiency by providing lower power dissipation and higher power-to-weight densities. The CLTM12-S provides improved safety and reliability while reducing equipment downtime, overall vehicle weight, and wiring complexity.

About TTI

TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of interconnect, passive and electromechanical (IP&E) components and the distributor of choice for industrial and consumer electronics manufacturers worldwide. Broader and deeper inventory, leading-edge products and custom supply chain solutions have established TTI as the leading specialist in electronic component distribution. Globally, the company maintains over 2 million square feet of dedicated warehouse space containing over 850,000 component part numbers. Along with its subsidiaries, Mouser Electronics, Sager Electronics, and TTI Semiconductor Group, TTI employs more than 7,000 people at more than 133 locations throughout North America, South America, Europe, Asia and Africa. For more information about TTI, visit www.ttiinc.com