Fort Worth, Texas – September 9, 2019 – TTI, Inc., a leading specialty distributor of electronic components, has stock for immediate shipment of multiple values of the Eaton Bussmann High Speed fuses, also called “semiconductor fuses” to reference what they are protecting. Ranging from 50-400 amp, these 500V AC/DC compact fuses use up to 48 percent less enclosure space when compared with traditional high speed, round body fuses. The innovative design allows for a significantly smaller package without compromising heat rise performance. Other sizes are available from 130-1,000V AC/DC and up to 4,000A.
Round-body bolted style high-speed fuses are the most common in North America for protecting power semiconductor devices. Semiconductor devices can withstand high currents for only an extremely short period of time. The overcurrent protective device selected must also limit the overvoltage during fault interruption. The only overcurrent protective device with all these qualities is the modern high-speed fuse, commonly referred to as a “semiconductor fuse” or “I2t fuse”).
Eaton’s Electrical Vehicle or EV fuses are specifically designed to protect sensitive electric and hybrid automotive equipment, including high voltage, high capacity batteries, power conversion equipment, contactors, cabling, and other auxiliary circuits. The EV fuses are available in four case sizes and protect high power battery charging and management systems up to 500 Vdc in ratings from 50 to 400 amps.
About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of interconnect, passive and electromechanical (IP&E) components and the distributor of choice for industrial and consumer electronics manufacturers worldwide. Broader and deeper inventory, leading-edge products and custom supply chain solutions have established TTI as the leading specialist in electronic component distribution. Globally, the company maintains 1.9 million square feet of dedicated warehouse space containing over 850,000 component part numbers. Along with its subsidiaries, Mouser Electronics, Sager Electronics, and TTI Semiconductor Group, TTI employs more than 6,700 people at more than 133 locations throughout North America, Europe and Asia. For more information about TTI, visit www.ttiinc.com
About Eaton
Eaton is a power management company with 2018 sales of $21.6 billion. We provide energy-efficient solutions that help our customers effectively manage electrical, hydraulic and mechanical power more efficiently, safely and sustainably. Eaton is dedicated to improving the quality of life and the environment through the use of power management technologies and services. Eaton has approximately 99,000 employees and sells products to customers in more than 175 countries.