Fort Worth, Texas – October 29, 2019 – TTI, Inc., a leading specialty distributor of electronic components, has stock for immediate shipment of the MAL219690113E3, a 90F, 2.8V Hybrid energy storage cap from Vishay.
The Vishay 196 HVC series exhibits more than three times the energy density of a traditional supercapacitor and is available in 4F, 15F and 90F versions. Useful life is up to 2000hr at 85°C and up 100,000 charge/discharge cycles. Additionally, the HVC series has a very low self-discharge rate, which can be less than 5 percent per month or less than 15 percent after three months.
196 HVC ENYCAP capacitors are approved up to 10 g for safe use in consumer, automotive, and industrial environments. ENYCAPs are available in various layouts (flat, stacked, pins, tabs) with a profile as low as 2.5mm. Voltages for the hybrid storage caps range from 1.4V for a single cell up to 8.4 volts for multiple cells.
Applications are wide-ranging and include memory power backup, real-time clock backup, write-cache protection for hard drives, burst power for flash lighting and wireless transmitters, energy harvesting storage devices and UPS power sources.
Search Vishay 196 HVC ENYCAP Supercapacitors
About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of interconnect, passive and electromechanical (IP&E) components and the distributor of choice for industrial and consumer electronics manufacturers worldwide. Broader and deeper inventory, leading-edge products and custom supply chain solutions have established TTI as the leading specialist in electronic component distribution. Globally, the company maintains 1.9 million square feet of dedicated warehouse space containing over 850,000 component part numbers. Along with its subsidiaries, Mouser Electronics, Sager Electronics, and TTI Semiconductor Group, TTI employs more than 6,700 people at more than 133 locations throughout North America, South America, Europe, Asia and Africa. For more information about TTI, visit www.ttiinc.com
About Vishay Intertechnology
Vishay Intertechnology, Inc., a Fortune 1,000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, rectifiers, MOSFETs, optoelectronics, and selected ICs) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.