Fort Worth, Texas – May 6, 2019 – TTI, Inc., a leading specialty distributor of electronic components, is now stocking the XRCGB Quartz Crystals from Murata.

Murata’s XRCGB SMD Type Quartz Crystals feature an original package technology to create compact high-quality (low ESR and impact-resistant) crystal units. Load capacitance is dependent upon user design, such as 6pF, 8pF or others.

The frequency range is 16.000 to 50.000MHz and features Murata’s proven package technology using a resin sealed package of 2.0x1.6x0.7mm, whereby reliability is enhanced using a particle screening process. They are ideal for consumer applications such as wireless communications (BLE/NFC), wired communications (Ethernet/USB), microcomputers, HDDs/SSDs, PCs, and healthcare equipment. 

Search Murata XRCGB Crystals

 

About TTI

TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of interconnect, passive and electromechanical (IP&E) components and the distributor of choice for industrial and consumer electronics manufacturers worldwide. Broader and deeper inventory, leading-edge products and custom supply chain solutions have established TTI as the leading specialist in electronic component distribution. Globally, the company maintains 1.9 million square feet of dedicated warehouse space containing over 850,000 component part numbers. Along with its subsidiaries, Mouser Electronics, Sager Electronics, and TTI Semiconductor Group, TTI employs more than 6,700 people at more than 133 locations throughout North America, Europe and Asia. For more information about TTI, visit www.ttiinc.com

 

About Murata

Murata is a global leader in the design, manufacture and supply of advanced electronic materials, leading edge electronic components, and multi-functional, high-density modules. Murata innovations can be found in a wide range of applications from mobile phones to home appliances, and automotive applications to energy management systems and healthcare devices.

Murata XRCGB