Fort Worth, Texas – June 25, 2019 – TTI, Inc., a leading specialty distributor of electronic components, is now stocking the TSOP95 and TSOP96 series receivers from Vishay. These devices deliver improved dark-ambient and disturbed-ambient sensitivity to infrared signals, better suppression of RF noise, and excellent pulse-width accuracy.

These new receivers are targeted at designs for a variety of remote control applications such as air conditioners, audio systems, video projectors, cameras, video game systems IR remote control in televisions, set-top boxes (STBs), and more. For the remote control function in these products, the devices are immune against disturbances such as IR emissions from CFL lamps and RF emissions from on-board Wi-Fi antennas. In addition, the modules’ improved pulse-width accuracy allows lower bit error rates for almost any code, and the devices are insensitive to supply voltage variations and ripple noise.

To streamline the design cycle, the receivers feature a photodetector, preamplifier circuit, and IR filter in a single 4-pin epoxy Heimdall (TSOP95) and Panhead (TSOP96) package. The devices are available with carrier frequencies from 30 kHz to 56 kHz and five automatic gain control (AGC) versions for short and long burst codes. The receivers feature a low supply voltage from 2.0 V to 3.6 V and a typical supply current of 0.37 mA. They are RoHS-compliant, halogen-free and Vishay Green.

Search Vishay Infrared Receivers

About TTI

TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of interconnect, passive and electromechanical (IP&E) components and the distributor of choice for industrial and consumer electronics manufacturers worldwide. Broader and deeper inventory, leading-edge products and custom supply chain solutions have established TTI as the leading specialist in electronic component distribution. Globally, the company maintains 1.9 million square feet of dedicated warehouse space containing over 850,000 component part numbers. Along with its subsidiaries, Mouser Electronics, Sager Electronics, and TTI Semiconductor Group, TTI employs more than 6,700 people at more than 133 locations throughout North America, Europe and Asia. For more information about TTI, visit www.ttiinc.com

 

About Vishay Semiconductor

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader.