Fort Worth, Texas – July 22, 2019 – TTI, Inc., a leading specialty distributor of electronic components, is now offering the SM13126PEL LAN 10/100 Base-Tx VoIP PoE Transformer from Bourns.
Bourns Inductive Components Product Line has introduced the Model SM13126PEL single-port, potted construction LAN 10/100 Base-Tx VoIP and IEEE 802.3 compliant transformer for Ethernet applications. This LAN transformer is PoE capable with an extended operating temperature range of -40 to +85ºC and 1.5k Vrms isolation voltage.
These transformers are perfect for applications needing voice and power delivered to an endpoint such as industrial paging systems, surveillance systems with speaker capability and VoIP phones. Having the ability to power and communicate using one cable greatly reduces installation cost and improves reliability for the entire life of the system.
Search Bourns SM13126PEL Transformers
About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of interconnect, passive and electromechanical (IP&E) components and the distributor of choice for industrial and consumer electronics manufacturers worldwide. Broader and deeper inventory, leading-edge products and custom supply chain solutions have established TTI as the leading specialist in electronic component distribution. Globally, the company maintains 1.9 million square feet of dedicated warehouse space containing over 850,000 component part numbers. Along with its subsidiaries, Mouser Electronics, Sager Electronics, and TTI Semiconductor Group, TTI employs more than 6,700 people at more than 133 locations throughout North America, Europe and Asia. For more information about TTI, visit www.ttiinc.com
About Bourns
Bourns, Inc., is a leading manufacturer and supplier of position and speed sensors, circuit protection solutions, magnetic components, microelectronic modules, panel controls and resistive products. Headquartered in Riverside, California, USA, Bourns serves a broad range of markets, including automotive, industrial, consumer, communications, non-critical life support medical, audio and various other market segments. Additional company and product information is available at www.bourns.com