Fort Worth, Texas – July 17, 2019 – TTI, Inc., a leading specialty distributor of electronic components, is now stocking the Murata LoRa Module Type ABZ (CMWX1ZZABZ).
Murata’s Type ABZ module is a new, compact, low cost, low power wide area network (LPWAN) wireless module that supports the LoRaWAN long-range wireless protocol. This new stand-alone module measures 12.5 x 11.6 x 1.76 mm, and is constructed in a metal shielded package and comprises a Semtech SX1276 ultra-long range spread spectrum wireless transceiver and an STMicro STM32L0 series ARM Cortex-M0+ 32-bit microcontroller (MCU). An integrated TCXO with robust low drift thermal characteristics provides an accurate clock source for the RF transceiver.
Communication with the module can be achieved via UART, SPI, or I2C peripheral interfaces. An ADC and up to 18 GPIOs provide plenty of flexibility for connecting sensors, switches and status LEDs. The module is powered from a 2.2 to 3.6 VDC supply. The Murata (CMWX1ZZABZ) module has pre-certified radio regulatory approvals for operating in the 868 and 915 MHz industrial, scientific and medical (ISM) spectrum in most geographical regions of the world.
About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of interconnect, passive and electromechanical (IP&E) components and the distributor of choice for industrial and consumer electronics manufacturers worldwide. Broader and deeper inventory, leading-edge products and custom supply chain solutions have established TTI as the leading specialist in electronic component distribution. Globally, the company maintains 1.9 million square feet of dedicated warehouse space containing over 850,000 component part numbers. Along with its subsidiaries, Mouser Electronics, Sager Electronics, and TTI Semiconductor Group, TTI employs more than 6,700 people at more than 133 locations throughout North America, Europe, and Asia. For more information about TTI, visit www.ttiinc.com
About Murata
Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture, and sale of ceramic-based passive electronic components & solutions, communication modules, and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world. For more information, visit Murata's website at www.murata.com