Fort Worth, Texas – January 24, 2019 – TTI, Inc., a leading specialty distributor of electronic components, is now stocking the TCUT1630 and TCUT1800 AEC-Q101 qualified 3 and 4 channel optical sensors from Vishay. These sensors are all targeted for turn and push, absolute and incremental encoding applications.

The triple-channel TCUT1630X01 includes an infrared emitter and three phototransistor detectors located across from each other in a surface-mount package. With a taller dome than previous-generation devices and an additional channel for a vertical push function or indexing tab, the device is ideal for turn and push encoding. The quad-channel TCUT1800X01 includes two infrared emitters and four phototransistor detectors, and can detect up to 16 positions for absolute and incremental encoding.

Both sensors just released can detect motion, speed, and direction. They can be used as position sensors for encoders in high temperature automotive environments, in addition to turn interior knobs, ignition locks, adaptive headlights, and electric power steering (EPS) systems. In industrial applications, these devices are ideal for monitoring gas or water meters and detecting the status of doors, panels, and inserted coins or credit cards.

Compatible with reflow solder processes according to JEDEC-STD-020D, these devices are RoHS-compliant, halogen-free, and Vishay Green.  Samples and production quantities of the optical sensors are available now, with lead times under 12 weeks for large orders.

The TCUT1630X01 and TCUT1800X01 deliver a typical output current of 1.3 mA and operate at a wavelength of 950 nm. The optical sensors feature a 3 mm gap width and apertures of 0.3 mm, and offer a wide temperature range of -40 °C to +105 °C. With a Moisture Sensitivity Level rating of 1 (MSL1), the TCUT1630X01 and TCUT1800X01 have an unlimited shelf life.

Search Vishay TCUT Optical Sensors

 

About TTI

TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of interconnect, passive and electromechanical (IP&E) components and the distributor of choice for industrial and consumer electronics manufacturers worldwide. Broader and deeper inventory, leading-edge products and custom supply chain solutions have established TTI as the leading specialist in electronic component distribution. Globally, the company maintains 1.9 million square feet of dedicated warehouse space containing over 850,000 component part numbers. Along with its subsidiaries, Mouser Electronics, Sager Electronics, and TTI Semiconductor Group. TTI employs over 6,000 employees and is represented in over 100 locations throughout North America, Europe and Asia. For more information about TTI, visit www.ttiinc.com

 

About Vishay Semiconductor

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. – TTI is fully franchised for Vishay Optoelectronic products. TTI's experienced customer service team members are ready to help you at 1-877-645-4TTI.

Vishay-Auto-optical_PR-Image