Fort Worth, Texas – February 14, 2019 – TTI, Inc., a leading specialty distributor of electronic components, is now stocking the BH1749NUC color sensor from ROHM Semiconductor, targeted at LCD backlight screen adjustment in control panels, tablets, cameras or mobile applications. Ideal market applications are industrial, medical, safety and security equipment.
The BH1749NUC is a uniquely packaged low profile surface mounted sensor. The operating voltage is 2.3V to 3.6V with an illuminance detection range of 80 klx (Typ) and operating temperature range of -40 °C to +85 °C. The sensor detects red, green, blue and infrared and is able to convert them to digital values. With a wide dynamic range and high sensitivity, this sensor is able to determine the illuminance and color very accurately, which is critical for automatic backlighting adjustments.
Search Rohm Semiconductor BH1749NUC Ambient Light Sensors
About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of interconnect, passive and electromechanical (IP&E) components and the distributor of choice for industrial and consumer electronics manufacturers worldwide. Broader and deeper inventory, leading-edge products and custom supply chain solutions have established TTI as the leading specialist in electronic component distribution. Globally, the company maintains 1.9 million square feet of dedicated warehouse space containing over 850,000 component part numbers. Along with its subsidiaries, Mouser Electronics, Sager Electronics, and TTI Semiconductor Group. TTI employs over 6,000 employees and is represented in over 100 locations throughout North America, Europe, and Asia. For more information about TTI, visit www.ttiinc.com
About ROHM Semiconductor
ROHM offers a full line of leading-edge sensors, silicon carbide MOSFETs and Schottky barrier diodes, optoelectronics, and power management ICs. If you’re designing for rugged environments requiring high-temperature and/or high-voltage along with higher power density solutions – TTI is fully franchised for ROHM, Kionix MEMS Sensors and accelerometers, and LAPIS Semiconductor products.