Fort Worth, Texas – August 9, 2019 – TTI, Inc., a leading specialty distributor of electronic components, is now stocking the APT2012 Series infrared emitters and detectors from Kingbright. These LEDs are targeted for unique sensing applications in Industrial and medical equipment applications. 

Kingbright’s IR LEDs selection with infrared, phototransistor and sensor industry standard SMD and through-hole packages features infrared emitter and phototransistor in the wavelength range from 880nm to 940nm @ 20mA (or *50mA) with different lens options and viewing angles from 20° to 160°. This selection offers multiple package alternatives which include PLCC, subminiature, top emitting, right angle, dome lens SMD LEDs, as well as 3mm and 5mm through-hole in matching emitter/detector pairs.

To further broaden our product offering, Kingbright introduces ambient light photo sensor and RGB color sensor. The ambient light photo sensor is a NPN silicon phototransistor which is adapted to respond to the human eye. Sensitive to visible spectrums, it is an effective power saving solution to display backlighting appliances. The RGB color sensor uses three Si photodiodes with color filter, which makes it an ideal solution to color balance of display backlighting appliances. Both sensors are available in SMD packages.

Search Knighbright APT2012 LEDs

 

About TTI

TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of interconnect, passive and electromechanical (IP&E) components and the distributor of choice for industrial and consumer electronics manufacturers worldwide. Broader and deeper inventory, leading-edge products and custom supply chain solutions have established TTI as the leading specialist in electronic component distribution. Globally, the company maintains 1.9 million square feet of dedicated warehouse space containing over 850,000 component part numbers. Along with its subsidiaries, Mouser Electronics, Sager Electronics, and TTI Semiconductor Group, TTI employs more than 6,700 people at more than 133 locations throughout North America, Europe and Asia. For more information about TTI, visit www.ttiinc.com

 

About Kingbright

Kingbright Company LLC has manufactured innovative Light Emitting Diodes for over 30 years. Kingbright offers the most comprehensive LED product portfolio in the industry, including SMD LEDs, thru-hole LEDs, SMD/through-hole displays, circuit board indicators and high brightness LEDs. Kingbright also offers fully customized LED solutions to enhance customer designs with many options in LED packaging and colors. www.kingbrightusa.com

Kingbright