Fort Worth, Texas – April 30, 2019 – TTI, Inc., a leading specialty distributor of electronic components, is now stocking the Rohm SML-D15 LED Series. These high-accuracy single-rank 1608-size high-brightness chip LEDs are optimized for industrial, medical and automotive systems.
The SML-D15 series was developed using a comprehensive, highly integrated manufacturing system (from device fabrication), allowing ROHM to exceed the limits of conventional LED production. As a result, high-accuracy brightness is achieved and brightness variations are reduced by 75 percent, making it possible to provide a single-rank of brightness, significantly easing the design challenges.
Additionally, by optimizing the LED die, ROHM is able to improve brightness by up to 3x over conventional products, delivering class-leading brightness in the 1608 size (1.6mm x 0.8mm). The LEDs are also AEC-Q101 qualified, making them suitable for medical and automotive applications demanding increased reliability.
About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of interconnect, passive and electromechanical (IP&E) components and the distributor of choice for industrial and consumer electronics manufacturers worldwide. Broader and deeper inventory, leading-edge products and custom supply chain solutions have established TTI as the leading specialist in electronic component distribution. Globally, the company maintains 1.9 million square feet of dedicated warehouse space containing over 850,000 component part numbers. Along with its subsidiaries, Mouser Electronics, Sager Electronics, and TTI Semiconductor Group, TTI employs more than 6,700 people at more than 133 locations throughout North America, Europe, and Asia.
For more information about TTI, visit www.ttiinc.com
About Rohm Semiconductor
ROHM Semiconductor is an industry leader in system LSIs, discrete components, and module products, utilizing the most advanced technologies and proprietary production systems. ROHM employs highly skilled individuals with expertise in all aspects of design, development, manufacture, sales and marketing.