Fort Worth, Texas – December 14, 2018 – TTI, Inc., a leading specialty distributor of electronic components, stocks a broad selection of ITT Cannon Trident Neptune Metal Connectors. The Trident Series is a versatile range of electrical connectors with fully interchangeable contacts, designed to excel in harsh environments. These rugged connection systems are an outstanding choice in applications that require additional shielding, sealing, and the extra durability of a metal shell.

ITT Cannon’s Trident Neptune Metal Series combines membrane seals and Universal Shielded Endball to create a cost-effective and easy to assemble connector solution. This series features nickel plated zinc alloy shells, IP67 sealing, and UL 94 V-0 rated thermoplastic insulators, allowing for an operating temperature from -55 °C to +105 °C. They are able to withstand approximately 200 mating cycles and meet UL 1977 and CSA C22.2 qualifications. The connectors are RoHS compliant and recognized under the component program of CSA.

To learn more visit https://www.ttiinc.com/content/ttiinc/en/manufacturers/f-i/itt-cannon/products/itt-cannon-trident-neptune-metal-tnm-series-connectors.html

About TTI

TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of interconnect, passive and electromechanical (IP&E) components and the distributor of choice for industrial and consumer electronics manufacturers worldwide. Broader and deeper inventory, leading-edge products and custom supply chain solutions have established TTI as the leading specialist in electronic component distribution. Globally, the company maintains 1.9 million square feet of dedicated warehouse space containing over 850,000 component part numbers. Along with its subsidiaries, Mouser Electronics, Sager Electronics, and TTI Semiconductor Group. TTI employs over 6,000 employees and is represented in over 100 locations throughout North America, Europe, and Asia. For more information about TTI, visit www.ttiinc.com

 

About ITT Cannon

ITT's Cannon brand is a leading global manufacturer of connector products serving international customers in the aerospace and defense, medical, energy, transportation and industrial end markets. Whether delivering critical specs to aircraft pilots, streaming data through communications satellites or giving expectant parents a first look at their unborn children, Cannon connects the world’s most important information to the people who need it. In 2015, Cannon celebrated 100 years of making connections that helped make history. Cannon products were used in the first “talking” movies and helped transmit the first messages home from the moon. Today we proudly continue our legacy of innovating to connect the world and inspire the successes of the next century – because amazing things happen when great things connect. For more information, visit www.ittcannon.com