Fort Worth, Texas – December 12, 2018 – TTI, Inc., a leading specialty distributor of electronic components stocks a complete line of Amphenol SV SMPM Connectors for high density, high-frequency applications. Offering microwave performance through 65 GHz and less than .140-inch center-to-center spacing, the connectors are ideal when minimum board separation width is needed.
SMPM Connectors are available in multiple configurations to accommodate any board-to-board spacing requirement and feature a “push-on” design for mating without the need for threads and wrenches. With higher withdrawal forces on the full dent shrouds, they have become a standard for quick and effective interconnects using both semi-rigid and flexible cables. The connectors are 20 percent smaller than the Amphenol SV Microwave SMP connectors.

About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of interconnect, passive and electromechanical (IP&E) components and the distributor of choice for industrial and consumer electronics manufacturers worldwide. Broader and deeper inventory, leading-edge products and custom supply chain solutions have established TTI as the leading specialist in electronic component distribution. Globally, the company maintains 1.9 million square feet of dedicated warehouse space containing over 850,000 component part numbers. Along with its subsidiaries, Mouser Electronics, Sager Electronics, and TTI Semiconductor Group. TTI employs over 6,000 employees and is represented in over 100 locations throughout North America, Europe, and Asia. For more information about TTI, visit www.ttiinc.com
About Amphenol SV Microwave
SV Microwave (cage code: 95077) is a world leader in the RF/Microwave industry with over 50 years of proven performance. We design and manufacture RF/Microwave coaxial connectors, cable assemblies and passive components designed for military, IoT, 5G, satellite, high speed, aerospace, commercial and telecommunications applications.