Jonathan Schultz is the captain of Team HUGE and lives in Conneticut. He first started building combat robots with Peter and Maddie. They brought brought 3 30lb robots to the North East Robotics Club (NERC) in 2017 and met Garrett and Don.
Peter Lombardo is a mechanical engineer working as an aerospace technical writer in Conneticut. He has a 30lb robot named BEEESS?? that competes in the sportsman class for NERC events, which has podiumed in 2017, 2018, and 2019. Peter does the electronics, and works on design and fabrication, including cutting the wheels.
Garrett Santoline has been building combat robots since his freshman year of high school and built several robots in a variety of weight classes. He lives in Georgia and works for the Air Force as a civilian employee. Garrett works on building and fixing the robot after bouts.
Don Doerfler is from Pittsburg PA, and started building robots in high school with Garrett. Don machines parts for HUGE and serves in the pit crew, as well as post-match diagnosis and taming the the wiring.
Maddie Thumma met John and Peter in college and serves as the unofficial team manager, managing logistics, as well as designing the graphics for HUGE, including the eyes. She works for Digital Retail Partners in Connecticut as a Ecommerce Manager and Graphic Designer.