Wheels: HUGE's wheels are 40 inches tall and made of Ultra High Molecular Weight (UHMW) plastic. They are flexible and bend, rather than break. This allows HUGE to be thrown around during the fight and not break. All the cutouts are done by hand and make the wheel lighter, without sacrificing durability.
Weapon Bar: The weapon bar is made of AR500 steel, and weighs 30 pounds. The team has a variety of lengths to use, which can be swapped out to hit opponents exactly where they want.
Steel Body: The body of HUGE is made of welded AR400 Steel which protects the electronics and batteries from damage during a match. Both sides of the body are mirrored to each other and can run independently.
Legs: HUGE's legs are made of UHMW, the same material as the wheels. If the legs were gone, HUGE would not be able to drive anywere and the main body would just spin freely between the wheels.
Titanium Bar: The poles coming out of the wheels are 1 inch thick titanium bars that are just extensions of the drive axle. They stick out so far from the wheels to keep HUGE from getting stuck sideways on a wheel in case it is flipped or knocked over.
Angry Eyes: The most important element of HUGE are the angry eyes. They send a signal to other teams to tell them that HUGE means business, and will show no mercy in the battle box.