Codes and Sizes of SMD Resistors

 Diagram Of SMD Resistors

What is an SMD Resistor?

SMD Resistors (Surface Mounted Device Resistors) are some of the tiniest parts you can buy, and they're only getting smaller. Here is how you can decipher case codes when you search TTI.com.

How to decipher codes and sizes for SMD Resistors:

SMD Resistor sizes are marked by a numerical code, such as 0603 for example. This code contains the width and height of the package. The code 0603 indicates a length of 0.060" and a width of 0.030" and is given in either imperial or metric units. 

Looking for SMD Resistors? Search TTI's Inventory