How does a Microswitch work?

 Diagram Of A Microswitch

What is a Microswitch and how does it work? 

Microswitches, also known as miniature snap-action switches, are electric switches actuated with very little physical force, using a tipping-point mechanism, or spring to open and close connections inside of them. Moving the spring-loaded actuator that rests on top of a plunger, causes the spring to snap back and forth, thus changing the direction of power quickly between two devices.

The three connection points Microswitches use:

Common leadnormally open lead, and normally closed lead. Power is typically attached to the common lead; this leads into the switch and energizes the spring. Because the normally closed lead is touching the spring, it sends power causing the resting state, meaning nothing is pushing against the activating actuator. When the actuator is moved, the spring snaps into a new position and then changes the path of power by sending it out the normally open lead.

 

Looking for Microswitches? Search TTI's Inventory