robot arm

In a world of smart phones and smart cities, creating a smart building offers the next opportunity for industry as controls for heating and air conditioning systems, lighting, refrigeration and many other factors utilize data and intelligence to upgrade traditional systems. Sensors for temperature, pressure and humidity can be utilized systems to wirelessly transmit actionable data from a wide variety of sources across a single building or an entire campus. From HVAC systems on a building rooftop to high-efficiency lighting systems that can be scheduled or even detect presence, Industrial Internet of Things (IIoT) solutions that rely on components from TE Connectivity and TTI are changing the factory environment. 

TTI logo
TE Connectivity logo

Be There with TTI and TE Connectivity

TTI, TE Connectivity and the Industrial
Internet of Things – Bringing Data to Work

Featured IIoT Products

Building Automation Resources

M3200 Pressure Transducer

Jim Zhang, TE Connectivity Product Manager for Pressure Sensors, discusses the trends driving more demand for digital pressure sensors, the comparisons of analog vs. digital sensors and key applications suited for digital sensors.

Piezoresistive Pressure Transducer

TE Connectivity Sensor Solutions Senior Product Development Engineer, Hai Mei, discusses the various benefits and applications of Microfused technology.

The Buchanan WireMate Connector

The TTI Specialist sheds some light on TE Connectivity’s Buchanan WireMate Connector Surface Mount TB Series. This two-piece pluggable SMT connector solution enables designers of lighting, controls and building automation systems to fully switch to SMT printed circuit boards.

Connected Homes and Intelligent Buildings Solving for Reliability, Convergence, Connectivity 

The concept of an automated home is not a new one: the idea has been floated since the 1930s at World’s Fair venues, and in popular culture as TV shows and movies imagine home life of the future – solidifying the public’s view of the benefits of home automation. 

Building Safety and Security Solutions

TE Connectivity’s comprehensive guide contains three essential documents that profile power and data connectivity solutions for a higher level of building safety and security.

The Importance of Pressure Sensors in HVACR Systems

Industrial Relays

Predictive Maintenance – Real-time Sensor Data from 200 Feet in the Air

Monitoring sensor output signals over a period of time can offer insights into equipment failure. From bearing vibration to rising temperatures, as properties change, the decline in performance or need for part replacement can be predicted to avoid catastrophic failure, downtime and cost. Filtration is another area of maintenance; as an example, differential pressure sensors can be used to monitor pressure across a filter to predict hydraulic or pneumatic filter maintenance. 

For industrial condition monitoring and predictive maintenance applications vibration specification parameters are considered critical to ensure long-term, reliable, stable and accurate performance including: wide frequency response, measurement resolution, low drift and operating temperature. 

Asset Monitoring – Inventory Data Directly from the Asset

Keeping raw materials in the production pipeline is key to optimizing your output. With the Industrial Internet of Things (IIoT) and TE Connectivity sensors from TTI, monitoring your production line to know the volume of available materials on hand can happen from virtually anywhere. This can be a tremendous benefit when measuring liquid levels in tank farms or food processing systems where distance, or sanitary conditions require remote sensing. By enabling the power of the IIoT, asset monitoring goes where you go. 

Process Automation – Position and Speed Data in Real-time

Industry 4.0 process automation relies on accuracy in data coming from the production line. TE Connectivity sensors from TTI allow instant, accurate information on the state of your system from the exact point you need it. Pressure, temperature, humidity and many other factors affecting your systems can be monitored allowing control and continuous operation without hands-on supervision. Leverage the power of the Industrial Internet of Things with TE Connectivity and TTI, to bring your data to work. 

TE Connectivity and TE connectivity (logo) are trademarks